Part Number: CC2564CMSP432BTBLESW
Other Parts Discussed in Thread: CC256XCQFN-EM, BOOST-CCEMADAPTER, CC3200
My setup:
CC256XCQFN-EM
MSP432P401R launchpad
BOOST-CCEMADAPTER
CC3200 AudBoost
Code Composer Studio Version: 10.4.0.00006
BT Stack: CC2564CMSP432BTBLESW-v5.1.1
My Questions: follows my previous thread here (All in HFP profile only, sometimes I can use HSP(if no choice on HFP))
1) Can I have a tonal indication functionality (beep sound played locally on the device side) upon BT connect / disconnect, Volume + or Vol -? if possible how? can I add the custom sound files to it?
2) One of my previous questions is in continuation to the previous thread is to send the command "AT+XEVENT=TALK,1\r" or "AT+XEVENT=TALK,0\r" under HFP profile only (HSP if HFP not possible)
Mr Jacob responded to my previous question to use the API below BTPSAPI_DECLARATION int BTPSAPI SPP_Data_Write(unsigned int BluetoothStackID, unsigned int SerialPortID, Word_t DataLength, Byte_t *DataBuffer);
if I understand well in order to use the above API to send the custom AT command under HFP I need to merge the examples of HFP & SPP profiles? & then use this above API rite? let me know
I'm just a bit confused can I also use the API "HFRE_Send_Arbitrary_Command();" ? function to achieve the same result (from Device ->AG )? or any other possibilities under HSP?
Thanks for your time.