Part Number: CC2640R2F
Other Parts Discussed in Thread: BLE-STACK
Good day! I am looking into Bluetooth-SIG RF-PHY testing for a custom project (based on simple_peripheral, using BLE-Stack from SDK 5.30.00.03) under QDID 135680.
Several questions were raised in working through the process:
- Host Test Settings -- SWRA601H (https://www.ti.com/lit/an/swra601h/swra601h.pdf) specifies that the host_test project can be used for SIG testing, assuming it utilizes the same "protocol stack and radio configuration." How would I compare protocol stack and radio configurations between projects? Which parameters or settings need to be identical?
- RF-PHY Features -- A test lab asked which RF-PHY features we are supporting, and provided the following list. Which features does the BLE-Stack simple_peripheral project support, or which parameters should I check to confirm our feature set?
-
LE Transmitter
-
LE Receiver
-
LE 2M PHY
-
Stable Modulation Index -Transmitter
-
Stable Modulation Index -Receiver
-
LE Coded PHY (Long Range)
-
Thanks for the help! I am new to Bluetooth, and did not originally develop the project, so there is a definite learning curve.
-Kenton