This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: SimplePeripheral works with RCOSC but not XOSC LF - custom board

Part Number: CC2640R2F


Hello,

I am having a somewhat odd issue. I have a custom board that I have flashed a modified version of SimplePeripheral to. I did all of the basic modifications in here to get it up and running, but it only works when I use the RCOSC build configuration. In addition, the system works as expected when using the LF XOSC (32khz clock) but ONLY if debugging with my XDS110. Otherwise, when not in RCOSC mode and not debugging, the system advertises but does not connect, and sometimes randomly restarts.

Some more information:

Yes, there are capacitors connected to the 32khz: 2 12pF caps.

My oscilloscope is broken and the board has no GPIO access, so I can't measure the clock speed by routing it through a DIO pin.

I am using SimpleLink 5.30.00.03 for CC2640r2, BLE5Stack, and TI-RTOS 2.21.01.08 with CCS v11

My custom board uses the 4mmx4mm variant of the CC2640R2F.