Part Number: CC2541
Other Parts Discussed in Thread: CC2540
I have recently (last moth or so ) bought a few HM-10 boards on Aliexpress with an cc2541 mcu on board. To my great surprise, when trieing to program the chip with my own firmware,
the SmartRF flash Programmer software (connected to a CCdebugger) reports the chip as an CC2540 and not as CC2541 as expected.
My firmware is utilizing the I2C and therefore I can't use the board if it is indeed an CC2540 instead of cc2541.
My questions are:
1. Does TI or anybody else are aware of such possible issue (the chip on these boards are marked with seemingly identical marking to chips on some HM-10 I bought in the past that works) ?
2. Is there a possibility/Application Note that utilize GPIOs for I2C communication instead of the on chip I2C ?
3. Does anybody knows of a reliable source of HM-10 with real CC2541.
4. Is there a reasonable(cheap and programmable) alternative to the HM-10