This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R7: Will HAP SDK (Homekit) work on the 2652R7 Silicon?

Part Number: CC2652R7

1. The HAP sdk mentions it supports CC26X2. I noticed the examples are configured for the 2642R1. I have a LP-CC26X2R1 that I was able to run the examples on. However, current design is to use the 2652R7 chipset. Do I just need to re configured the board files for the chip?

2. Is the HAP 4.10 SDK limited to the Simplelink 4.10 SDK or will the latest 6.x.x version work as well? 

Thank you, 

  • Hi,

    I have assigned your thread to a relevant expert. They will comment shortly.

    Best Regards,

    Jan

  • Hi Jonathan,

    1. Current version of the HAP SDK is only compatible with CC2642R1.

    2. Current version of the HAP SDK is only supposed to be used with SDK 4.10

    If not already done, I would recommend to reach out to your local support team to review the options available to you.

    Best regards,