This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: how to recompile the Hap SDK after modifying source files?

Part Number: CC2642R

Working with the homekit SDK hap_cc26x2_4_10_00_04. 

I want to modify the the GAP and GATT files included in this sdk to support non homekit functionality. However, I see code composer studio adds a binary to the project that isn't buildable. Didn't look like there was an option to modify the files before installing the SDK either. 

  • Hi,

    You can try to modify the project properties in order to build against the sources rather than the library.

    Please note that, in general, limited support is provided on public forums for MFI protected SDKs.

    I hope this will help,

    Best regards,