Part Number: CC2650
Hello,
I am having a similar issue as the poster of these two links:
CC2650: Unable to set TX power above 0dBm and Setting CC2650 TX Power
I am currently using a CC2650 Launchpad to test some changes which I hope to implement on a CC2650 chip used in an energy harvesting application.
Within CCS (8.2.0), I have changed DEFAULT_TX_POWER defined in ble_user_config.c from 7 to 12 (I have tried all values actually) but have not been able to see a change in the RSSI for any such value. From the first link referenced above, it seems that RSSI might not actually be the best way to measure an improvement in TX gain. How can I go about measuring the current in the antenna on the launchpad? I have access to an oscilloscope but am not sure across which resistor I can place the probes.
Additionally, I have read that one can use HCI commands to set the output power: HCI_EXT_SetTxPowerCmd(HCI_EXT_TX_POWER_5_DBM)
However, where does one call this? I think it should be called in the application folder, but do I call it in scTask, project_zero, or another file? And if so, where in these files? My understanding of the BLE stack is quite weak at the moment, but from the CC2650 datasheet, CC26X0 Developer's guide and Simplelink academy I have not been able to figure out this problem.
Thank you in advance for the help.
PR.