This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC13XX-CC26XX-SDK: Error building Simple Broadcast and Simple Peripheral

Part Number: SIMPLELINK-CC13XX-CC26XX-SDK

When trying to build the Simple Broadcast or the Simple Peripheral example, I get the following errors:
gmake: *** No rule to make target 'build-295672945', needed by 'configPkg/compiler.opt'.
gmake: *** No rule to make target 'build-295672945', needed by 'configPkg/linker.cmd'.
gmake: Target 'all' not remade because of errors.
gmake[1]: *** [build-295672945-inproc] Error -1073741701

SimpleLink CC13X2 CC26X2 SDK v13.10.0.53
XDCtools v3.51.2.21
TI v18.12.1.LTS
CCS v12
Windows 11
Acer Swift 3

Imported the example project using Project -> Import CCS Project.

Thank you in advanced for your help.

Akbar