Other Parts Discussed in Thread: LP-XDS110, LP-EM-CC2340R5, UNIFLASH
Hi,
Already refer to the last section image update example in the docs. (/cfs-file/__key/communityserver-discussions-components-files/538/CC23xx_5F00_BootLoader_5F00_draft.pdf)
I modified the cc13xx-sbl tool to program CC2340.
The UART of LP-EM-CC2340R5 can be directly used for programming without using LP-XDS110.

However, I have question during the implementation.
After completing the BLDR_CMD_CHIP_ERASE command. All main flash bank sectors not protected by FCFG1 and CCFG protect bits will be erased. The CCFG will be erased once the bank erase has completed.
When the CCFG erased, CCS and uniFlah will display an error message(Error -1274 @ 0x0)
Workround:
1. I have built the CC2340 example (host_test), which can be burned into the LP-XDS110 + LP-EM-CC2340R5 EVM board using CCS.
2. Then use uniFlash to export data.
host_test_512k.bin (512K bytes), address range: 0x0 - 0x7FFFF
ccfg.bin (2K bytes), address range: 0x4e020000 - 0x4E0207FF
Where to find bin file & CCFG file???
Is there an easy way to generate bin file & CCFG file?
May I ask if the mass production will still be burned in this way?
Thanks,
Aries