Other Parts Discussed in Thread: LP-XDS110, LP-EM-CC2340R5, UNIFLASH, CC2340R5
Hi,
I have built the CC2340 example (host_test), which can be burned into the LP-XDS110 + LP-EM-CC2340R5 EVM board using CCS.
It is hoped that the UART of LP-EM-CC2340R5 can be directly used for programming without using LP-XDS110.

Q1: Is it possible to use Flash Programmer 2 or Uniflash tool to burn it?
Q2: Is there any sample code that can be programmed via UART? (bootloader mode)

Thanks,
Aries