Other Parts Discussed in Thread: UNIFLASH
I'm trying to setup a CC1352P7-1 launchpad as a sniffer to test, but I have issues getting the flash programmer 2 and smartRF Sniffer 2 to detected the board.
I have tried all the method on the site, but no avail.
First question, when using the SmartRF Flash Programmer 2 to update firmware, there would be enumeration failed.

second question, I can use UniFlash to connect my board, and update C:\Program Files (x86)\Texas Instruments\SmartRF Tools\SmartRF Packet Sniffer 2\sniffer_fw\bin\cc1352p1lp\sniffer_fw.hex

However, It can not detect device by SmartRF Sniffer Agent - v1.7.0. ( I've also tried v1.5.0, v1.8.0, v1.9.0, but it doesn't work)