This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In one of my Project we are currently using CC2652 in one of our Project.
As per new additional requirement we need to add up Amazon Sidewalk functionality.
As mentioned in Ti site CC2652R7 & CC2652P7 SoCs are compatible with Amazon Sidewalk:
I wanted to understand:
1) Is It possible to Run Amazon Sidewalk & BLE simultaneously within Single application.
2) If yes what modifications are needed
Hi Shubhendu,
The Sidewalk stack is already capable of commissioning and communicating over the BLE PHY. If you require simultaneous Sidewalk and BLE applications then you should be aware that there are no existing efforts within TI to create a DMM solution with these stacks projects. It should be feasible to accomplish given both projects consume less than half of the available 704 kB of flash memory on the CC2652X7 devices, however this effort would need to be undertaken by the developer.
Regards,
Ryan