This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Power consumption question

Part Number: CC2340R5

Dear Expert

Testing power consumption using basic_ Ble_ LP_ EM_ CC2340R5_ Freertos_ The configuration file for the ticlang project is basic_ The ble.syscfg file contains many parameters that are not understood in BLE configuration. Is there any reference material to learn in this area, such as how to configure MITM's pinKey. There is also the parameter under "Connection Update Request Params". After I made the changes, the power consumption did not change after the connection was successful. The connection interval seems to have been 50ms, isn't it changed here? There is also the interval for broadcasting, which is only useful by changing the "Primary PHY Interval Minimum" parameter. Changing the "Advertising Interval Value (ms)" parameter under "Advertising Interval" is not useful, and I have some doubts about the parameter configuration here; In addition, there are some new projects and other issues that need to be consulted with FAE.
In addition, our PCB board has returned and needs to be adjusted later on. Could you please help me check the attached principle and PCB wiring for the antenna part.