Part Number: CC2564C
Other Parts Discussed in Thread: CC2564
In CC2564C datasheet, a note said the HFP and A2DP cannot be supported simultaneously, does this mean we can not switch these two modes freely? E.g. the smartphone is playing music through BT classic headset, and there is a incoming call, can we switch to the call and answer that via headset?
The CC2564C device uses the coprocessor to perform the LE functionality or to execute the assisted HFP 1.6 (WBS) or assisted A2DP functions. Only one of these functions can be executed at a time because they all use the same resources (that is, the coprocessor; see Table 3-1 for the modes of operation supported by each device).