Part Number: CC2564C
We're interested in concurrent A2DP and HFP so users can easily switch between music and phone calls when using the CC2564C chip. According to the datasheet "The assisted modes (HFP 1.6 and A2DP) are not supported simultaneously. Furthermore, the assisted modes are not supported simultaneously with Bluetooth low energy". So we would need to run in unassisted mode on one of either A2DP or HFP. Is there a recommendation on which should remain in assisted and which we should support externally in unassisted mode?