This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: How to salvage bricked XDS110 of the Launchpad?

Part Number: LAUNCHXL-CC1352R1


Hello!

I was playing with LAUNCHXL-CC1352R1. I have built ProjectZero and was going to load it over JTAG using CCS. A window popped proposing something like update Stellaris firmware, to which I agreed. After that the Launchpad's emulator seems to be bricked. Plugged and unplugged, tried different USB port, rebooted computer - whatever I do it does not appear in computer's device manager. Another Launchpad seems to work, though on different COM port (5 and 6, the bricked one was on 9 and 10). I have seen XDS110SupportReadMe.pdf, the last page was about my case. There is instruction to put it into DFU mode by grounding JTAG TDO pin. The manual tells to ground pin 97. I have attempted to ground TDO pin on XDS110 to CC1352 header from the emulator side, connected Launchpad to USB, but it still is not recognized as USB device.

Please advise how to salvage the board.

Thanks