This guide shows how to use SDK Composer so the size of the SDK downloaded and installed is reduced.
This guide applies to the devices supported by the SimpleLink Low Power F2 SDK (CC13x1, CC13x2, CC13x4, CC26x1, CC26x2 and CC26x4) and SimpleLink
Low Power F3 SDK (CC23xx).
1- Open https://dev.ti.com/tirex/. This web-page centralizes the development resources (SDK, training, documentation, etc.) for all the TI devices.
2- Unroll the "Wireless connectivity" > "Embedded Software". This should display several SDKs. Hover over the SDK applicable to your device, click on the three dots and on "Download".
The screenshot below shows the procedure for the Low Power F2 SDK.

3- A pop-up is displayed and invite you to select the components you need.
Select the components you want (this automatically deselect the full download). Once done, click the download icon and eventually the "Done" button.
The screenshot below shows how to create

4- This should automatically start the download of a zip file.
5- Extract the content of the zip file inside the C:\ti folder
6- The SDK is ready to be used!
Tip: In the SDK installation folder, the docs and examples folders can be deleted to save more space.
I hope this will help,