Part Number: CC2652R7
Hello,
I have noticed that if I build the same project consecutively without changing the code, the hex files are completely different. It seems to be related to CCS v12.7 which I am currently on because when I was on CCS v12.6 and this wasn't an issue. So I'm wondering is there is a setting I can toggle to fix this or if I should just revert to the older version. Also using the SDK I am using is 7_40_00_77.
Thanks,
Kenneth Thomas