Tool/software:
Hi,
Currently I am working on basic_ble Peripheral profile project. I have few queries on Attribute table and related issues.
// Initialize GATT attributes
GGS_AddService(GATT_ALL_SERVICES); // GAP GATT Service
So, right now I have used GGS_AddService(GATT_ALL_SERVICES) to add the GAP GATT Service which is implemented by the TI BLE Stack and following characteristics is added:
Generic Access 0x1800 // primary service
1. DEVICE_NAME_UUID 0x2A00 // Device Name
2. APPEARANCE_UUID 0x2A01 // Appearance
3. PERI_CONN_PARAM_UUID 0x2A04 // Peripheral Preferred Connection Parameters
4. CENTRAL_ADDRESS_RESOLUTION_UUID 0x2AA6 // Central Address Resolution
5. RESOLVABLE_PRIVATE_ADDRESS_ONLY_UUID 0x2AC9 // Resolvable Private Address Only
So, In my application I need to remove other characteristics from GAP GATT Service. So, Is there any way to remove Attribute with UUID 0x2AA6 from the GAP GATT Service (Service UUID - 0x1800)?
Thanks & Regards
Vignesh.