Part Number: CC2340R5
Tool/software:
Hi,
Chipset used: CC2340R5
SDK: simplelink_lowpower_f3_sdk_8_10_01_02
I am currently working on developing a BLE client application on the CC2340R5. I have been successful in scanning, connecting and service discovery. After doing service discovery I have successfully received the response along with some data. I am currently facing issues with making sense of the data that I have received from the service discovery response.
For additional info of my project, Please refer this ticket.
I am running the Data stream example provided the SDK on a CC2340R5 since it is configured to be a peripheral. I have another CC2340R5 EVK on which I running the basic BLE example code in CLIENT role.
Below is a screenshot taken from nrf connect of the services exposed by the data stream example.

After a connection is done, I am calling the "GATT_DiscAllPrimaryServices' API. Details of how I am calling the api is explained in the ticket link which I have shared at the beggining.
Once I get a "ATT_READ_BY_GRP_TYPE_RSP" Event, I print the len and numGroups fields as shown below.

The contents of the message are as follows.
0x01,0x00,0x0b,0x00,0x00,0x18,0x23,0x00,0xff,0xff,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0xb0,0x00,0x40,0x51,0x04,0xc0,0xc0,0x00,0xf0
Help me understand the above packet.