Part Number: CC2340R5-Q1
Other Parts Discussed in Thread: LP-XDS110ET, SYSCONFIG
Tool/software:
Hi teams,
We are now testing the frequency on EVM to familiar with the test operation. This allows us to test the custom board as soon as it arrives.
1. In our test, we found that when we choose "disable", "use board setting" and "enable with Q1=Q2=35", the frequency is totally the same. I would like to know how much capacitance the internal capacitor contributes to the Cload when “disable” is selected.
2. Now, we use the LP-XDS110ET through the USB to connect SmartRF 8 on PC. Can we also connect the SmartRF 8 through the USB-to-Uart port on the custom board?
3. We also try to use the btool HCIExt_ModemTestTxCmd,. We already set Q1=Q2=0 in Sysconfig. but the frequency is faster 40KHz than "SmartRF 8 enable with Q1=Q2=0" (both are channel 39 & 0 dbm Tx power). Should they show the same frequency in the test or there's still another reason causing the difference between HCIExt_ModemTestTxCmd & SmartRF. If so, should we refer to btool or SmartRF 8 in our design?
4. In SamrtRF 8, does RF compensation is the default open?
5. We'll send our custom board to the crystal vendor for Crystal Circuit Evaluation. Is the Crystal working when the power supply is on? Or any mode you recommend when testing the crystal itself?
These are extensions of the previous question.
CC2340R5-Q1: Crystal cap_array tuning - Bluetooth forum - Bluetooth®︎ - TI E2E support forums
Many thanks,
Jesse