Tool/software:
Hi,
Our application uses mcuboot + dual image, with SimpleLink Low Power F3 SDK 8.20.00.119.
During production testing, we encountered an issue:
When using the default NVS settings, everything functions normally.
On the second boot, execution reaches the program area in about 2 seconds.
However, if NVS is modified, the system takes three boots before stabilizing at 2 seconds.
This issue only occurs on the first programming of a brand-new CC2340R5.
Once the CC2340R5 has been programmed and run at least once, the issue does not reoccur.
Questions:
Is this behavior avoidable?
Is there a way to reset CC2340R5 to factory mode via software, without desoldering the chip?
I tried Chip Erase in UniFlash, but it didn't work.
A software-based reset would greatly simplify future testing.
Below are the NVS modifications I made:
Hi,
Out of curiosity, have you tried upgrading to the latest SDK to see if this persists?
Is there a way to reset CC2340R5 to factory mode via software, without desoldering the chip?
I tried Chip Erase in UniFlash, but it didn't work.
A mass erase should erase everything on the device. Just to clarify, once you've done a mass erase on the chip, data is still on flash?
A software-based reset would greatly simplify future testing.
This does exist. See here: https://dev.ti.com/tirex/content/simplelink_lowpower_f3_sdk_8_40_00_61/docs/drivers/doxygen/html/_power_8h.html#a1db423246eb4407154df05d8fedbf746
On the second boot, execution reaches the program area in about 2 seconds.
However, if NVS is modified, the system takes three boots before stabilizing at 2 seconds.
I'm a bit confused, do you mind elaborating what you mean by the system takes three boots before stabilizing at 2 seconds?
Best,
Nima Behmanesh
Hi,
Since we have already entered the product verification phase, it is not suitable to switch to a different SDK at this time.
Apologies for my previous brief description. Recently, I conducted further tests and found that when flashing firmware with modified NVS settings onto a blank IC, the first power-on is always affected. However, if the firmware is reflashed, this issue does not reoccur.
Device Boot Process:
Observed Behavior:
I captured power consumption data using a current meter, and it appears that both NVS writes and SPI transmissions are affected on the first boot. This causes proper NVS read/write operations and SPI control to function only on the second boot.
Questions:
Does modifying the NVS address region require the system to rewrite corresponding information?
How can we prevent this overlap from causing control failures during the first boot?
Hi,
Yes, NVS writes usually are preceded with an invalidate, and then a write to next available NVS memory section:
Additionally, NVS will disable interrupts and executing code in flash: NVSLPF3.h File Reference
So it makes sense why SPI may not work if the NVS is writing information to the device.
Apologies for my previous brief description. Recently, I conducted further tests and found that when flashing firmware with modified NVS settings onto a blank IC, the first power-on is always affected. However, if the firmware is reflashed, this issue does not reoccur.
By first power-on is always affected, you mean that it takes a little longer to execute?
Best,
Nima Behmanesh
Hi,
By first power-on is always affected, that not just by a longer execution time, but by a failure to write default values to NVS.
This issue only occurs when flashing firmware with modified NVS address regions. (We tested the same project code, changing only the NVS configuration.)
We are unsure what specific processes occur during the first boot after flashing firmware with modified NVS addresses onto a blank IC, leading to NVS write failures.
Additionally, we need guidance on how to prevent this issue from happening.
This problem has already caused false detections in our ATE program, so we would greatly appreciate your support in resolving it.
Hello,
I apologize for the delay, I was out sick last week.
I think I'm understanding the problem better now. If it's a blank chip and doesn't use the default NVS settings included in our projects, there are issues writing to it on the first boot. After the second, third boot than writing occurs normally.
If my understanding is incorrect, please let me know. I'll need to reach out to the drivers team to see what the process is. In parallel, I'll try this myself.
Here are the steps I'm going to do to try to reproduce:
1. Take a blank CC2340R5 and flash it using modified NVS settings
2. Read the NVS,
3. If it's blank write something to it
If the issue is reproduced, then the writing should fail on the first boot.
Is that right?
Best,
Nima Behmanesh
Hi Ian,
A couple of questions before I get started today trying to reproduce the issue:
1. Are you using NVS and external flash?
2. What compiler are you using?
These will help me rule out some variables that could be causing this issue.
Best,
Nima Behmanesh
Hello,
I've tested the NVS on an empty project, and I'm not seeing any issues. This leads me to believe that may be something involving the BLE stack. Are you calling the NVS APIs before or after the stack has initialized? In what function in the application are you calling the NVS APIs?
I will try it on my own, but knowing where you are calling these APIs (based on the diagram you provided earlier) I'll be able to reproduce the issue more quickly.
Best,
Nima Behmanesh
Hi,
I think your reasoning is valid. In my program flow, broadcasting and other operational parameters are stored in NVS, so I need to retrieve these parameters before initializing the BLE stack. Therefore, the NVS API calls occur before BLE stack initialization.
However, I noticed that osal_snv_init only executes after icall is initialized. Even if I manually call it earlier, it does not take effect.
Is there a way to initialize NVS before BLE stack initialization, ensuring I can access stored parameters?
Here is my code snippet.
Hello,
I tried the same test on basic_ble, but reading/writing NVS before the stack is initialized, and I'm not seeing any issues. I did this by modifying the appMain function in app_main.c:
NVS_Handle region1; NVS_Params nvsParams; uint8_t buf[32] = {0}; void appMain(void) { NVS_init(); GPIO_init(); NVS_Params_init(&nvsParams); region1 = NVS_open(CONFIG_NVS_0, &nvsParams); int_fast16_t status = 0; status = NVS_read(region1, 0, buf, 1); if (status != NVS_STATUS_SUCCESS) { GPIO_write(CONFIG_GPIO_LED_RED, 1); while(1); } if (buf[0] == 0xFF) { status = NVS_write(region1, 0, 0, 1, NVS_WRITE_POST_VERIFY); if (status != NVS_STATUS_SUCCESS) { GPIO_write(CONFIG_GPIO_LED_GREEN, 1); while(1); } } // Call the BLEAppUtil module init function BLEAppUtil_init(&criticalErrorHandler, &App_StackInitDoneHandler, &appMainParams, &appMainPeriCentParams); }
Note that I'm doing the reading and writing before the stack has initialized.
Best,
Nima Behmanesh
Hello,
Yes, I’ll try this tomorrow and get back to you.
Best,
Nima Behmanesh
Hello,
I've noticed something in trying to reproduce the issue:
Initially, I ran this code:
uint8_t buf[32] = {0}; void App_StackInitDoneHandler(gapDeviceInitDoneEvent_t *deviceInitDoneData) { bStatus_t status = SUCCESS; status = osal_snv_read(BLE_NVID_CUST_START, 4, buf); if (status != SUCCESS) { MenuModule_printf(10, 0, "FAILED READING!"); } status = osal_snv_write(BLE_NVID_CUST_START, 4, buf); if (status != SUCCESS) { MenuModule_printf(10, 0, "FAILED WRITING!"); }
I believe this code reproduced what you're seeing, that on a blank device the read fails the first time, and then on the second reset it is successful.
However, if we add a while(1); in the error handling for osal_snv_read() call, it will always fail when the chip was initially blank.
If we switch the calls, calling osal_snv_write before osal_snv_read():
uint8_t buf[32] = {0}; void App_StackInitDoneHandler(gapDeviceInitDoneEvent_t *deviceInitDoneData) { bStatus_t status = SUCCESS; status = osal_snv_write(BLE_NVID_CUST_START, 4, buf); if (status != SUCCESS) { MenuModule_printf(10, 0, "FAILED WRITING!"); } status = osal_snv_read(BLE_NVID_CUST_START, 4, buf); if (status != SUCCESS) { MenuModule_printf(10, 0, "FAILED READING!"); while(1); }
It will succeed without any issues.
This leads me to the following conclusion:
If the memory at BLE_NVID_CUST_START is empty (or any ID for that matter), then osal_snv_read() will return failure. However, if something is written to BLE_NVID_CUST_START (or any other ID), then osal_snv_read() will be successful.
In your program, you first read and if its blank you write. The issue is that osal_snv_read will return failure if what its reading is blank. After a mass erase, everything is blank, so reading anything will always fail. I'm also working on the assumption that on a read failure, you do not block the program from execution and continue to write (please let me know if my understanding is incorrect, and if it is, then we'll need an example project of some sort to reproduce it). This means that on the second boot, that ID has something written to it. In the documentation there is this quote:
No prior initialization of a NV item ID is required; the OSAL SNV manager initializes the NV ID when first accessed by a successful osal_snv_write() call.
Additionally, if we take a look at the example code given in the documentation:
status = osal_snv_read(SNV_ID_APP, BUF_LEN, (uint8 *)buf); if(status != SUCCESS) { Display_printf(dispHandle, dispIndex, 0, "#%5d SNV READ FAIL: %d", dispIndex, status); dispIndex++; //Write first time to initialize SNV ID // Because the osal_snv_read failed, we assume it's empty so we write something // to it, to initialize the ID. osal_snv_write(SNV_ID_APP, BUF_LEN, (uint8 *)buf); }
We see that if a osal_snv_read fails, then the assumption is that the ID has nothing written to it. This makes sense, since an ID is initialized once a successful osal_snv_write is called.
Here are a couple of solutions:
1. If the osal_snv_read fails, then you can assume that it's blank.
2. You can define your own NVS region and use the NVS driver. Once you've stored whatever you want in NVS, you can use osal_snv_write/read to load that information in the BLE NVS region. If it's bond information, then you can use the gapbondmgr APIs to import that bond.
I hope that helps!
Best,
Nima Behmanesh