Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hello expert,
Our customer will use RF output signals which are PAEN / LNAEN on their system board.
They want to get CPU interrupt by these signal edge.
The easy way is, to use these RF output pins as "Output" , then connect these pins to another "Input" GPIO.
However , for this case, it requires 2 pins for each (PAEN and LNAEN)
Instead of using 2 pins, is is possible to assign those RF signal port assigned GPIO as Output/Input, so that they can use GPIO edge interrupt by using only one pin?
Regards,
A.Fujinaka