Hello, during our use of the TI Bluetooth chip (model: CC2340R52E0WRHBRQ1), we encountered a wake-up failure issue with the Bluetooth temperature sensor. After analysis and troubleshooting, we found that this failure is caused by the reset phenomenon of the sensor — the reset forces the sensor to stay in a continuous data transmission state. This constant data transmission leads to continuous power consumption, and eventually, the sensor cannot wake up once the power is drained.
We also investigated the root cause of the reset phenomenon and finally confirmed that it is induced by MCU abnormality. Relevant materials are attached for reference: Attachment 2attachment 2.pdf includes partial investigation reports, and Attachment 1 attachment 1.pdf is the schematic diagram of the Bluetooth module. Please help analyze and troubleshoot this MCU abnormality. Thank you!