Part Number: CC2340R5
I am developing an app and have to work a lot with power modes. I have traced a problem all the way back to the basic_ble exmple. When I check the project property "Allow power transitions while running if supported (low power running)", I can no longer load the project onto the eval board. The loading dialogs spin forever. Turn the property off and everything loads but I never see the chip go into standby mode when it should. I have never seen the example consume less than 1.2 ma. I need to consume much less power in standby for my product. The following is a picture of the dialog I see when I set the property on.