This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI,
I am using the SPPLEDemo and running on CC256x QFN EM board with TM4C123G.
After I start the Server Mode:
SPP+LE>RegisterSPPLE
Sucessfully registered SPPLE Service.
SPP+LE>AdvertiseLE 1
GAP_LE_Advertising_Enable success.
After that I use my iPhone to connect the board, I can see the BD_ADDR of my iPhone from the console, then I can pair with my iPhone:
SPP+LE>
etLE_Connection_Complete with size 16.
Status: 0x00.
Role: Slave.
Address Type: Random.
BD_ADDR: 0x7548b694ef35.
SPP+LE>
etGATT_Connection_Device_Connection with size 16:
Connection ID: 1.
Connection Type: LE.
Remote Device: 0x7548b694ef35.
Connection MTU: 23.
SPP+LE>
SPP+LE>pairle 7548b694ef35
Attempting to Pair to 0x7548b694ef35.
GAP_LE_Request_Security returned 0.
SPP+LE>
etLE_Authentication with size 36.
Pairing Request: 0x7548b694ef35.
IO Capability: lcKeyboardDisplay.
MITM: TRUE.
Bonding Type: Bonding.
OOB: OOB Not Present.
Encryption Key Size: 16.
Sending Keys:
LTK: YES.
IRK: YES.
CSRK: YES.
Receiving Keys:
LTK: YES.
IRK: YES.
CSRK: YES.
Sending Pairing Response to 0x7548b694ef35.
GAP_LE_Authentication_Response returned 0.
SPP+LE>
etLE_Authentication with size 36.
latConfirmationRequest.
Invoking Just Works.
SPP+LE>
etLE_Encryption_Change with size 8.
SPP+LE>
etLE_Authentication with size 36.
Encryption Information Request 0x7548b694ef35.
Calling GAP_LE_Generate_Long_Term_Key.
Encryption Information Request Response.
GAP_LE_Authentication_Response (larEncryptionInformation) success.
SPP+LE>
etLE_Authentication with size 36.
Encryption Information from RemoteDevice: 0x7548b694ef35.
Key Size: 16.
SPP+LE>
etLE_Authentication with size 36.
Pairing Status: 0x7548b694ef35.
Status: 0x00.
Key Size: 16.
Then I try the discover the service by ANCS's UUID and I can't see the expected result:
SPP+LE>
Service 0x0003 - 0x0000, UUID: 5a7f.
Any idea? Many thanks for any reply!
Hi,
SPPLE is not a standard Bluetooth Profile. You will have to make sure the app can use the custom UUIDs that are needed to communicate and read and write to the app.
See the below post, similar discussion has happened http://e2e.ti.com/support/wireless_connectivity/f/660/p/375347/1329710.aspx