Other Parts Discussed in Thread: CC2640, CC2650
Hi,
I have SmartRF06 Evaluation Board and CC2650EM-7ID Module.
I have setup the CCS IDE and I am able to "Import" and "Build" the SimpleBLEPeripheral Project.
The BLE Stack Version is ble_cc26xx_2_00_00_42893 from where I have Imported the SimpleBLEPeripheral Project.
I am also able to flash the output hex file on the board but then the LCD is not showing anything and I am also not able to see any advertisement packets.
I am able to see the Red LED for Advanced Mode ON.
When I saw the Build Option in the CCS IDE, the variant is for CC2640, but I have the CC2650EM-7ID Module on the SmartRF06 Evaluation Board.
So this does not have any issues right (Please see the below snap) ?
I see that the Debugger stops at main(). I am also able to step-in to the functions and step-over the functions.
I am able to go till SimpleBLEPeripheral_createTask(), but then I do not see the SimpleBLEPeripheral_taskFxn() getting called and also the SimpleBLEPeripheral_init().
Please do let me know if I am missing anything.
Thanks,
Sunny