This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640:help port SimpleBLEPeripheral into 5x5

Other Parts Discussed in Thread: CC2640

 I am porting SimpleBLEPeripheral into 5x5 CC2640 with customized HW . However, the program seems cannot run as the debugger halts at the BIOS_start();getting this error message: No source available for "0x100035a2" ,i have followed the below reference site but do nothing help,any information for help, ths!http://e2e.ti.com/support/wireless_connectivity/bluetooth_low_energy/f/538/t/406173#pi239031350=1

In board.c

PIN_Config BoardGpioInitTable[] = {

    Board_LED1       | PIN_GPIO_OUTPUT_EN | PIN_GPIO_HIGH   | PIN_PUSHPULL | PIN_DRVSTR_MAX, 

    PIN_TERMINATE                                                                               /* Terminate list                */
};


and,modifying the compiler search path,remove the define xTI_DRIVERS_LCD_INCLUDED & xTI_DRIVERS_SPI_DMA_INCLUDED