This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Connection Terminate with 0x05/0x16 during bonding request.

Other Parts Discussed in Thread: CC2540

Hello, 

I am using CC2540 USB BLE Dongle with PC Application implemented in .Net.

Following Bond parameter has been set during initialization of this dongle.

GAPBOND_PAIRING_MODE -> 01-GAPBOND_PAIRING_WAIT_FOR_REQ
GAPBOND_MITM_PROTECTION -> 00-Disabled
GAPBOND_BONDING_ENABLED -> 01-Enabled
GAPBOND_IO_CAPABILITIES -> 03-No I/p No O/p

We are facing some issues in bonding when connected with the central devices, and receiving terminate command with reason code 0x05 in peripheral device.

But the Central device receiving terminate command with reason code 0x16.

This teminate command with reason code with 0x05/0x16 is not occuring when connection happening with pairing request.

After the devices gets paired, in the next connection with Bonding the devices, after connection establishment, terminate happens.

Kindly let us know the possiblity of the terminate connection with reason code 0x05 during bonding request.

Also please let us know is there any work arround or solution to resolve the problem with his terminate connection.


Note:

When we flash the host test image with bonding enabled, the issues is not occurring till some 10+ central devices get connecting with it.

After that we start receiving termination command with 05, once the connection gets established.

Regards,

Ramesh Kumar