This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650 problems with Smart RF flash programmer

Other Parts Discussed in Thread: CC2650, CC2640

Hi everybody,

I've just started with the CC2650 launchpad, and I test it with the "ProjectZeroApp_CC2650LAUNCHXL" and "ProjectZeroStack_CC2650LAUNCHXL". At the Code composer it works fine and the program runs, but when I try to program the Launchpad, using the "SmartRF Flash Programmer 2" tool, although write process finish successfully, nothing occurs. The program doesn't run.

Furthermore, everytime that I switch betwen Flash programmer and Code Composer, it's necessary a firmware update.

When I try to write through Flash Programmer, the next alert appears:


And, when I try to debug the program with Code Composer, appears:




My versions are:

Code Composer ver. 6.1.2.00015

TI-RTOS ver. 2.13.0.06

"cc26xx_bluetooth_smart__2.01.00.44423" files.

SmartRF Flash Programmer 2 ver. 1.7.2


Surely I'm not doing all steps properly, can somebody help me with this issue?

Thanks.