This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564 FCC Testing - Regarding Modulation & Test Pattern

Other Parts Discussed in Thread: CC2564MODN

This question is regarding the modulation type and test pattern values needed for FCC testing.

I have gone through the below links so far

I understand that I can use VS_Enable_FCC_Test_Mode() in Bluetopia SDK to put the chip in test mode.

int  VS_Enable_FCC_Test_Mode(unsigned int BluetoothStackID, VS_Modulation_Type_t Modulation_Type, Byte_t Test_Pattern, Byte_t Frequency_Channel, Byte_t Power_Level, DWord_t Generator_Init_Value, DWord_t EDR_Generator_Mask)

Unfortunately, I am unable to figure out what is the significance of modulation type and test pattern. I understood from HCI_VS_DRPb_Tester_Con_TX (0xFD84) that possible values for modulation type are

  • CW - Test pattern (second parameter, below) MUST be set to “All 1” or “All 0”
  • GFSK (BR)
  • π/4-DQPSK (2-EDR)
  • 8DPSK (3-EDR)
  • BLE

and test pattern are

  • PN9
  • PN15
  • 5555 (0101 0101 0101 0101b)
  • All 1
  • All 0
  • FOFO (1111 0000 1111 0000b)
  • FF00

How can I decide which to use for my testing purposes? Is there a documentation available on when to choose what?