This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I will begin teaching a course based on the CC2650 Launchpad next week and I am having trouble setting up the current version of CCS (6.2 for Windows for Simplelink Wireless) and the Simplelink Academy. I am trying to come up with install instructions that will allow students to build and run Project Zero.
CCS 6.2 installed without a problem. Resource Explorer is a new version that seems to ignore products installed in the installation directory, instead offering to download products from the cloud. I was able to install BLE from the cloud (It also installed TI-RTOS 2.13 and a version of the XDC tools). But I was not able to build and run the stack and app projects for Project Zero. Not from the cloud from Resource Explorer, and not from a local install of the Simpelink Academy. Many errors in both cases.
The cloud version (no local CCS) did work, but it has only this one example, not other examples for BLE or for TI-RTOS.
Any help would be appreciated. What I need is basically a set of components that if installed cleanly, would allow importing Project Zero as well as other BLE and TI-RTOS examples.
Thanks, Sivan Toledo
Hello Sivan ,
Please check under View -> Resource Explorer Classic for the local SimpleLink Academy 1.10 installation. I recommend doing a native install of CCS v6.2.0 Build 50 or later.
For best practices, please make sure to follow the guidance for installing the proper TI Compiler version. Also, remember to clear the phone's BT cache when switching firmware builds on the LAUNCHXL-CC2650 or you may fall victim to endless frustration
Beyond that, please do let us know how the class goes!
Best wishes