This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: Add Array data structure using Sensor Controller Studio

Part Number: LAUNCHXL-CC2650

How to add an array data structure using Sensor Controller Studio. I can create variables but no array.

The drop down in "Array Size" show only one option ("Not Array"). Please refer below image.

Please provide the procedure to add array.

  

  • You need to create a constant, ex : ARRAY_SIZE =64 in the upper right window. Then when you create data structure, the array_size part will be a drop down window with choice as not array or the array_size constant you just created.