Other Parts Discussed in Thread: CC2650,
Tool/software: TI-RTOS
In an effort to update my BLE application to a more recent version of TI-RTOS I completely messed up and deleted the projectzero_stack project folder which my custom BLE project based on projectzero used. Now I wanted to import the project again, however the resource explorer does not have the version anymore which I used for my project (seems like everything from 2650 is replaced by 2640r2). This is version 2.13.00.06.
My plan was to use the newer project zero for CC2650 with simplelink academy version 1.11. This one uses TI-RTOS 2.20. However, when I imported this project and tried to run it, it didn't advertise anything. So please, can someone help me get project zero back which used version 2.13 of TI-RTOS since I can't seem to find the location where I can download an older version of simplelink-academy (the version before 1.11). Or can someone tell me why it doesn't advertise in version 2.20, that would work as well. Anyway, thanks in advance.