Other Parts Discussed in Thread: CC2650,
Tool/software: Code Composer Studio
I just purchased a CC2640r2 Launchpad, and started using it. When I ran the SimpleBLE_peripheral program its working fine. Previously I was using CC2650 Launchpad but due to the flash memory issue I purchased a CC2640r2. In cc2650 I interfaced Oled SSD1306 in sensortag program.
As sensortag is based on SIMPLEBLE_peripheral So I decided to add the OLED SSD1306 driver in CC2640r2f SimpleBLE_peripheral Example. But when I added this I got following error
"C:/ti/simplelink_cc2640r2_sdk_1_50_00_58/source/ti/blestack/common/cc26xx/ccs/cc26xx_app.cmd", line 292: error #10099-D: program will not fit into available memory. run placement with alignment fails for section ".stack" size 0x400 . Available memory
I am not why am I getting this error. Right now I have large amount of flash memory but still getting this error in application stack. I tried to search about the error but I did not find any solution. I switched from CC25650 to CC2640r2 just because of memory but still getting the same error. Kindly look into issue. Thank You