Part Number: CC2640R2F
Hello!
We have a iOS app already live at customers which connects to our BT Dongle with CC2640R2F on board.
The pairing is tested and working on different iDevices except the latest iPhones, like the 8 and X until recently, which has BT5 (using a Broadcom BCM4361 wireless combo chip).
The issue we have on the iPhones 8 and X are that the pairing dialog comes up, but gets dismissed instantly, like the connection attempt is closed directly after it is been made.
I have tried nRF Connect, Bluesee and LightBlue, which all behaves the same.
Still it is not 100% failing all the time, since sometimes the pairing dialog stays after a reconnect but then fails afterwards.
Also I had out of 3 dongles, one connecting properly for a few times, but failed to work after that as well.
We received word that from our external testers, that they had a few iPhones X's which actually worked.
I tested an iPhone X out of the box with that current software version and the newest afterwards with no difference.
Also one thing to note is that we had access to 1 android device with BT5 and that one did not have any connection issues.
Our embedded systems engineer is momentarily not at the office, but I wanted to open this issue already for this is an urgent issue.
Thank you for your time!
Best regards,
Henk-Martijn Leidelmeijer