I have a CC2640 based board which was working fine since last 6 months or so. Today I programmed these devices again using JTAG and out of 6 devices, 2 devices got bricked.
The behaviour is something similar to this thread. When I insert a 3V coin cell, VDDS is held at 1.8V. VDDR is also at 1.8V. Reset line is also at 1.8V.
If I manually keep CC2640 in reset, VDDS returns to 3V but immediately after releasing the reset, it drops to 1.8V. So CC2640 is holding VDDS at 1.8V.
Can someone explain what can create such issues?
Thanks
Vinod