Other Parts Discussed in Thread: CC1352R, CC2640
Hi
I had a few questions regarding smartRf studio.
1. Why changing the packet interval does not make difference in the delay between each packet transmission and what is the minimum interval? How to set it? Because GUI does not work.
In the RX device, I am receiving packets every 100ms and does not matter what packet interval I set in the TX.
2. In BLE 4.2 and 5.0 in data channels packets can be up to 255 Bytes but the limited packet size in here in from 7-37. Is there any way to increase it?
3. How to record the log file in the transmitter or receiver? There is no save option.
I would be appreciated if you could kindly help.
Regards