Part Number: CC2650
Having an issue with the SPP client code.
I am trying to get it to connect to my bluetooth on a linux setup which is discoverable, i have added a line of code in accordance with the advice of the presvious person to help me however it would only run if i put it on like this:
uint8_t peerAddr[6] = { 0xb8, 0x27, 0xeb, 0x8d, 0xbb, 0xb2 };
The mac address of linux bluetooth im trying to get the client to connect to is: B8:27:EB:8D:BB:B2
The code runs and when i run the debug and open a serial connection the termial shows the correct message of: Hello from SPP BLE Client! With Data Length Extension support! Auto connecting...
However it does not connect to anything.
Can anyone please help? I am uploading the code from the SPP_BLE_Client file below.