Dear Sir,
We will like to ask following two questions.
1. Non-linear issue b/w ant1 vs. ant3
When we measure antenna pair of the TI CC2540R2 SimpleLink™ Angle of Arrival BoosterPack, the measurement result of pair ant 1 and ant 2 is liner. the pair ant 2 and ant 3 is liner too. but not pair ant1 and ant3.
The measurement of pair ant1 and ant3 is not as liner as the other two pairs. is it unknown issue?
Plus, in the TI AoA project, the pair ant 1 and ant 3 isn't used in the angle calculation. is there any particular reason why not using it as part of angle calculation?
2. Increase antenna spacing (from 0.5 -> 0.6 waveform length)
We will like to increase the waveform length from 0.5 to 0.6.
For my understanding, we can achieve this goal by increase the distance between antenna pairs.
If this is the case, how could we calculate the distance between the antenna pair to get the 0.6 waveform length?
The TI AoA antenna pair is 3.5cm.