This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: central get RSSI of advertising data,RSSI value is very unstable

Part Number: CC2640R2F

Hi,

I  get RSSI periodly with 2640R2F based on simple central example. The distance between central and advertising device is fixed.

Rssi changes very frequently,range could be larger than 15dB.

At the same time, Rssi monitored on mobilephone is stable.

What may be the.root cause? Thanks