Part Number: BOOSTXL-AOA
I know that can depend on a lot of environmental factors, but just curious what the ballpark response should be?
At 2m out we're getting 10-15 degree offsets and 20-40 degree swings.
Works great within 1 m though.
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BOOSTXL-AOA
I know that can depend on a lot of environmental factors, but just curious what the ballpark response should be?
At 2m out we're getting 10-15 degree offsets and 20-40 degree swings.
Works great within 1 m though.
thanks
Hi,
The SDK 2.40.00.32.
Thanks for the post reference. For the RTLS post seems like the last two could be applicable but they are 2.30.00.32.
Looking at the code, looks like these have been included in 2.4. Should I assume these 2.3 fixes are included in 2.4?
Also, we would like to run two BOOTXL-AOAs to try actual location. Will the demo work with using the same PC and slave device?
Thanks,
michael