Part Number: LAUNCHXL-CC2640R2
Hi,
I tested the long range functionality using 2 CC2640r2 Launchpad using BLE5 simple broadcaster and central project (simplelink_cc2640r2_sdk_3_10_00_15).
Configs:
Tx Power: 5dBm
.primPhy = GAP_ADV_PRIM_PHY_CODED_S2,
.secPhy = GAP_ADV_SEC_PHY_CODED_S2,
With This configuration and in General mode of advertising I can see the advertising data only till 250m.(with LOS).
So please let me know
1)Is there any other configuration do I need to do .
2)Is TI has any test report regarding the same?