Part Number: CC2640R2F
Other Parts Discussed in Thread: ENERGYTRACE
Tool/software: Code Composer Studio
Hello,
I have issues with the "Bad Energy Trace data was detected in the data stream" error when using the Energy Trace HDR add on.
From looking at other tickets the answer seems to be that CCS cannot keep up with the sampling rate; which is an explanation but not a resolution.
Any suggestions? With this error the XDS110 ADD-ON ENERGY TRACE HDR device is basically unusable.
Also, I've noticed for the samples I do capture they are far noisier than with the basic XDS110 Energy Traceset up. I was doing a comparison with just a lone 300k ohm resistor and noticed a wild amount of noise on with the add on that I don't see with the basic set up. Is this expected?
Jason