Part Number: CC1352R
Hi,
We are working with CC1352R Custom board and LAUNCHXL-CC1352R1. We are using following tools:
1. SDK V3.40.00.02
2. CCS9.3.0
3. iOS LightBlue Application
4. Our custom board: CC1352R1F3 TI 98J E. PD2T G4
5. LAUNCHXL-CC1352R1: CC1352R1F3 TI 98J E. PD30 G4
We have used simple peripheral OAD onchip application example code.
1. On our own custom board, I can scan "SP OAD on-chip" through LightBlue application but when I am trying to connect peripheral, but I come across a problem about establishing BLE connection:
According to debug information from serial port, when BLE link is established, it is disconnecting immediately. So I could not able to connect the peripheral through LightBlue application.
2. On LAUNCHXL-CC1352R1, I have flashed same application code. I can scan "SP OAD on-chip" through LightBlue application and I can connect peripheral successfully and everything is ok.
I have adjusted capacitor array on our custom board and we have checked and verified the frequency error is less or equal than 20 ppm, but the same problem is still there. Now I don't know what is the problem? Can you give me some good suggesions or guide to sovle this problem?
Thank you very much!
BRs.