Part Number: CC2652R
Tool/software: Code Composer Studio
The min CTE interval is 100ms, can we set it to 10ms or 20 ms
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
From a spec point of view, you can have a CTE at the end of each connection packet. The minimum connection interval is 7.5ms. So you could send a CTE at the end of each connection packet, i.e. with 7.5ms of interval.
However you have to consider other elements too:
I hope this will help,
Best regards,