This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We have some questions about the CC2510 input port’s dynamic behavior (there is basically nothing in the datasheet).
BTW, this is one of the ordinary PIOs, specifically PIO1_2, not one of the two special PIOs, PIO1_0 and PIO1_1, that don’t have pullup/pulldown.
Assume Vdd = 3.0V, room temp, port configured for input and not pulled up or down internal.
At the minimum
Thanks,
Adam
Hi,
I am afraid these parameters will be difficult to dig up for this device.
Please use the absolute maximum ratings of the device from datasheet and conduct some tests suitable for the application case.
regards