This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC1352P7: Unable to get Audio output from I2S echo example.

Part Number: LP-CC1352P7
Other Parts Discussed in Thread: CC3200AUDBOOST, CC3200, CC1352P7, CC2652R7, CC2642R

Hi,

   I was trying to run I2S echo example shared by TI resource .

The example recommends the CC3200AUDBOOST, which i purchased and followed the steps as below:

CC3200 Audio BoosterPack

  • The BoostPack’s DIN signal pin is not compatible with this LaunchPad. Use one of the following modification(s) to enable the CC3200 Audio BoosterPack’s usage with the i2secho example.
  • Bend down the two pins below DIO30. Additionally bend down DIO28-30. Be sure that the bent pin(s) do not make contact with the IC or any other component, bend them enough to make sure they don’t connect to the CC3200 Audio BoosterPack.
  • Attach the CC3200 Audio BoosterPack to the LP_CC1352P7_4
  • Run jumper wires between the following pins on the CC3200 Audio BoosterPack:
    • DIN: P3.3 and P3.9
    • DOUT: P3.4 and P3.10
    • BCLK: P3.5 and P3.8
    • FSYNC/WCLK: P4.9 and P3.7
I Did the first 3 steps and checked if i need to do step 4. Then i saw that connections should lead to "NC"(No connection, which i ensured by bending pins.
I ensured the 3.3V pin pointer matching to Launchpad pointer as well, as you can see in image attached.
With this setup, when i flash I2S example, i can see driver initialization LED glowing on CC1352P7 launchpad, but the audio feedback i am not getting.
What other way i can debug this ?
Attaching the photo of my setup.
  • Dear Vinay,

    I found two problems in the i2secho example:

    First, The INPUT_OPTION and OUTPUT_OPTION defines are ignored, and used nowhere else in the project.

    Secondly, it is going to sound counterintuitive, but in order to get the microphone working and outputting to the Line out output, you have to use the following call:

     /* Configure Codec */
        status =  AudioCodec_config(AudioCodec_TI_3254, AudioCodec_16_BIT,
                                    SAMPLE_RATE, AudioCodec_STEREO, AudioCodec_SPEAKER_HP,
                                    AudioCodec_MIC_ONBOARD);

    Let me know if it solved your issue.

    Regards,

    Arthur

  • One additional information is : When i change onboard microphone in i2s example code (without any changes), it works.

    So now the code of mine should be reviewed and set accordingly . 

    Can you please review and let me know.

    /*
     * Copyright (c) 2015-2020, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /*
     *  ======== i2secho.c ========
     */
    #include <stdint.h>
    #include <stddef.h>
    #include <stdint.h>
    
    /* POSIX Header files */
    #include <pthread.h>
    #include <semaphore.h>
    
    /* Driver Header files */
    #include <ti/drivers/GPIO.h>
    #include <ti/drivers/I2S.h>
    
    /* Driver configuration */
    #include "ti_drivers_config.h"
    #include "AudioCodec.h"
    
    #define THREADSTACKSIZE   2048
    
    /* The higher the sampling frequency, the less time we have to process the data, but the higher the sound quality. */
    #define SAMPLE_RATE                     16000   /* Supported values: 8kHz, 16kHz, 32kHz and 44.1kHz */
    #define INPUT_OPTION                    AudioCodec_MIC_ONBOARD //AudioCodec_MIC_MONO //AudioCodec_MIC_LINE_IN
    #define OUTPUT_OPTION                   AudioCodec_SPEAKER_HP
    
    /* The more storage space we have, the more delay we have, but the more time we have to process the data. */
    #define DATA_15sec      SAMPLE_RATE*2*1.5 // 48Kbytes, assuming 16bit PCM and 1.5sec worth data.
    #define NUMBUFS         188      /* Total number of buffers to loop through */ /*NUMBUFS = DATA_15sec/256*/
    #define BUFSIZE         256     /* I2S buffer size */
    #define BUFFER_15sec    NUMBUFS*BUFSIZE
    
    /* Semaphore used to indicate that data must be processed */
    static sem_t semDataReadyForTreatment;
    static sem_t semErrorCallback;
    
    /* Lists containing transactions. Each transaction is in turn in these three lists */
    List_List i2sReadList;
    List_List treatmentList;
    List_List i2sWriteList;
    
    /* Buffers containing the data: written by read-interface, modified by treatment, and read by write-interface */
    # if 0
    static uint8_t buf1[BUFSIZE];
    static uint8_t buf2[BUFSIZE];
    static uint8_t buf3[BUFSIZE];
    static uint8_t buf4[BUFSIZE];
    static uint8_t buf5[BUFSIZE];
    static uint8_t buf6[BUFSIZE];
    static uint8_t buf7[BUFSIZE];
    static uint8_t buf8[BUFSIZE];
    static uint8_t buf9[BUFSIZE];
    static uint8_t buf10[BUFSIZE];
    static uint8_t* i2sBufList[NUMBUFS] = {buf1, buf2, buf3, buf4, buf5, buf6, buf7, buf8, buf9, buf10};
    
    /* Transactions will successively be part of the i2sReadList, the treatmentList and the i2sWriteList */
    I2S_Transaction i2sTransaction1;
    I2S_Transaction i2sTransaction2;
    I2S_Transaction i2sTransaction3;
    I2S_Transaction i2sTransaction4;
    I2S_Transaction i2sTransaction5;
    I2S_Transaction i2sTransaction6;
    I2S_Transaction i2sTransaction7;
    I2S_Transaction i2sTransaction8;
    I2S_Transaction i2sTransaction9;
    I2S_Transaction i2sTransaction10;
    static I2S_Transaction *i2sTransactionList[NUMBUFS] = {&i2sTransaction1,  &i2sTransaction2,  &i2sTransaction3,
                                                           &i2sTransaction4,  &i2sTransaction5,  &i2sTransaction6,
                                                           &i2sTransaction7,  &i2sTransaction8,  &i2sTransaction9,
                                                           &i2sTransaction10};
    #endif
    
    static uint8_t buffer_15sec[BUFFER_15sec]; // Buffer worth of 1.5sec with sample rate of 16KHz.
    I2S_Transaction i2sTransaction_15sec[NUMBUFS]; // hold i2sTransaction of 188 size, each worth of 256bytes
    static I2S_Transaction *i2sTransactionList[NUMBUFS];
    
    I2S_Handle i2sHandle;
    
    static void errCallbackFxn(I2S_Handle handle, int_fast16_t status, I2S_Transaction *transactionPtr) {
        /* The content of this callback is executed if an I2S error occurs */
        sem_post(&semErrorCallback);
    }
    
    static void writeCallbackFxn(I2S_Handle handle, int_fast16_t status, I2S_Transaction *transactionPtr) {
        /*
         * The content of this callback is executed every time a write-transaction is started
         */
    
        /* We must consider the previous transaction (the current one is not over)  */
        I2S_Transaction *transactionFinished = (I2S_Transaction*)List_prev(&transactionPtr->queueElement);
    
        if(transactionFinished != NULL){
            /*
             * Remove the finished transaction from the write queue and feed
             * the read queue (we do not need anymore the data of this transaction)
             */
            //List_remove(&i2sWriteList, (List_Elem*)transactionFinished);
            //List_put(&i2sReadList, (List_Elem*)transactionFinished);
    
            /*
             * We do not need to queue transaction here:
             * treatment-function takes care of this :)
             */
        }
    }
    
    static void readCallbackFxn(I2S_Handle handle, int_fast16_t status, I2S_Transaction *transactionPtr) {
        /*
         * The content of this callback is executed every time a read-transaction
         * is started
         */
    
        /* We must consider the previous transaction (the current one is not over) */
        I2S_Transaction *transactionFinished = (I2S_Transaction*)List_prev(&transactionPtr->queueElement);
    
        if(transactionFinished != NULL){
    
            /* The finished transaction contains data that must be treated */
            /*List_remove(&i2sReadList, (List_Elem*)transactionFinished);
            List_put(&treatmentList, (List_Elem*)transactionFinished);*/
    
            if(transactionPtr == i2sTransactionList[NUMBUFS-1])
            {
                    volatile uint32_t dummy = 10; // Add a break point on this line
            }
    
    
            /* Start the treatment of the data */
            sem_post(&semDataReadyForTreatment);
    
            /*
             * We do not need to queue transaction here:
             * writeCallbackFxn takes care of this :)
             */
        }
    }
    
    /*
     *  ======== echoThread ========
     */
    void *echoThread(void *arg0)
    {
        /* Initialize TLV320AIC3254 Codec on Audio BP */
        uint8_t status = AudioCodec_open();
        if( AudioCodec_STATUS_SUCCESS != status)
        {
            /* Error Initializing codec */
            while(1);
        }
    
        /* Configure Codec */
        status =  AudioCodec_config(AudioCodec_TI_3254, AudioCodec_16_BIT,
                                    SAMPLE_RATE, AudioCodec_MONO, AudioCodec_SPEAKER_HP,
                                    //AudioCodec_MIC_ALL);
                                    AudioCodec_MIC_ONBOARD);
                                    //AudioCodec_MIC_LINE_IN);
        if( AudioCodec_STATUS_SUCCESS != status)
        {
            /* Error Initializing codec */
            while(1);
        }
        printf("\n----------------Hello-------------------------\n");
        /* Volume control */
        AudioCodec_speakerVolCtrl(AudioCodec_TI_3254, AudioCodec_SPEAKER_HP, 75);
        AudioCodec_micVolCtrl(AudioCodec_TI_3254, AudioCodec_MIC_ONBOARD, 75); //AudioCodec_MIC_ONBOARD
    
        /* Prepare the semaphore */
        int retc = sem_init(&semDataReadyForTreatment, 0, 0);
        if (retc == -1) {
            while (1);
        }
    
        /*
         *  Open the I2S driver
         */
        I2S_Params i2sParams;
        I2S_Params_init(&i2sParams);
        i2sParams.samplingFrequency    =  SAMPLE_RATE;
        i2sParams.fixedBufferLength    =  BUFSIZE;
        //i2sParams.writeCallback      =  writeCallbackFxn ;
        i2sParams.readCallback         =  readCallbackFxn ;
        i2sParams.errorCallback        =  errCallbackFxn;
        i2sParams.SD0Use               = I2S_SD0_DISABLED;
        i2sParams.SD1Channels          = I2S_CHANNELS_MONO;
    
        i2sHandle = I2S_open(CONFIG_I2S_0, &i2sParams);
        if (i2sHandle == NULL) {
            /* Error Opening the I2S driver */
            while(1);
        }
    
        /* Initialize the queues and the I2S transactions */
        List_clearList(&i2sReadList);
        List_clearList(&treatmentList);
        //List_clearList(&i2sWriteList);
    
        uint8_t k;
        for(k=0;k<NUMBUFS;k++){
            i2sTransactionList[k] = &(i2sTransaction_15sec[k]);
        }
        /* Half the transactions are initially stored in the read queue */
        for(k = 0; k < NUMBUFS; k++) {
            I2S_Transaction_init(i2sTransactionList[k]);
            i2sTransactionList[k]->bufPtr  = &(buffer_15sec[k*BUFSIZE]); //i2sBufList[k];
            i2sTransactionList[k]->bufSize = BUFSIZE;
            List_put(&i2sReadList, (List_Elem*)i2sTransactionList[k]);
        }
    
        /* The second half of the transactions is stored in the write queue */
    #if 0
        for(k = NUMBUFS/2; k < NUMBUFS; k++) {
            I2S_Transaction_init(i2sTransactionList[k]);
            i2sTransactionList[k]->bufPtr  = i2sBufList[k];
            i2sTransactionList[k]->bufSize = BUFSIZE;
            List_put(&i2sWriteList, (List_Elem*)i2sTransactionList[k]);
        }
    #endif
    
    
        I2S_setReadQueueHead(i2sHandle,  (I2S_Transaction*) List_head(&i2sReadList));
        //I2S_setWriteQueueHead(i2sHandle, (I2S_Transaction*) List_head(&i2sWriteList));
        List_tail(&i2sReadList)->next = List_head(&i2sReadList); /* I2S buffers are queued in a ring-list */
        List_head(&i2sReadList)->prev = List_tail(&i2sReadList);
    
        /* Start I2S streaming */
        I2S_startClocks(i2sHandle);
        I2S_startRead(i2sHandle);
        //I2S_startWrite(i2sHandle);
    
        /* Treatment */
        while(1){
    
            /* Wait for transaction ready for treatment */
            retc = sem_wait(&semDataReadyForTreatment);
            if (retc == -1) {
                while (1);
            }
    
            I2S_Transaction* transactionToTreat = (I2S_Transaction*) List_head(&treatmentList);
    
            if(transactionToTreat != NULL){
                /*
                 * Treatment:
                 *   The higher the sampling frequency,
                 *   the less time we have to process the data
                 */
                #if SAMPLE_RATE > 16000
                    /* No data processing */
                #elif SAMPLE_RATE > 8000
                    /* Data processing */
                    int16_t *buf = transactionToTreat->bufPtr;
                    /* bufSize is expressed in bytes but samples to consider are 16 bits long */
                    uint16_t numOfSamples = NUMBUFS * transactionToTreat->bufSize / sizeof(uint16_t);
                    uint16_t n;
                    /* We only modify Left channel's samples () */
                    //for(n=0; n<numOfSamples-2; n=n+2) {
                        /*
                         * Here we use a very basic filter
                         * (average to reduce noise level on left channel)
                         *
                         * Note: data coming from left channel and right channel
                         * are interleaved
                         */
                        //buf[n] = (buf[n] + buf[n+2]) / 2;
                    //}
                #else
                    /* Data processing */
                    int16_t *buf = transactionToTreat->bufPtr;
                    uint16_t numOfSamples = transactionToTreat->bufSize / sizeof(uint16_t);
                    uint16_t n;
                    /* We modify both channel's samples */
                    for(n=0; n<numOfSamples-2; n=n+1) {
                        /*
                         * Here we use a very basic filter (average to reduce noise level)
                         *
                         * Note: data coming from left channel and right channel
                         * are interleaved
                         */
                        buf[n] = (buf[n] + buf[n+2]) / 2;
                    }
                #endif
    
                /* Place in the write-list the transaction we just treated */
                List_remove(&treatmentList, (List_Elem*)transactionToTreat);
                //List_put(&i2sWriteList, (List_Elem*)transactionToTreat);
            }
        }
    }
    
    /*
     *  ======== mainThread ========
     */
    void *mainThread(void *arg0)
    {
        pthread_t           thread0;
        pthread_attr_t      attrs;
        struct sched_param  priParam;
        int                 retc;
        int                 detachState;
    
        /* Call driver init functions */
        I2S_init();
    
    /* On CC32XX, do not enable GPIO due to an LED/I2S pin conflict */
    #if !(defined(DeviceFamily_CC3200) || defined(DeviceFamily_CC3220) || defined(DeviceFamily_CC3235))
        GPIO_init();
    
        /* Configure the LED pin */
        GPIO_setConfig(CONFIG_GPIO_LED_0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
    
        /* Turn on user LED */
        GPIO_write(CONFIG_GPIO_LED_0, CONFIG_GPIO_LED_ON);
    #endif
    
        /* Set priority and stack size attributes */
        pthread_attr_init(&attrs);
        priParam.sched_priority = 1;
    
        detachState = PTHREAD_CREATE_DETACHED;
        retc = pthread_attr_setdetachstate(&attrs, detachState);
        if (retc != 0) {
            /* pthread_attr_setdetachstate() failed */
            while (1);
        }
    
        pthread_attr_setschedparam(&attrs, &priParam);
    
        retc |= pthread_attr_setstacksize(&attrs, THREADSTACKSIZE);
        if (retc != 0) {
            /* pthread_attr_setstacksize() failed */
            while (1);
        }
    
        /* Create receive thread */
        retc = pthread_create(&thread0, &attrs, echoThread, NULL);
        if (retc != 0) {
            /* pthread_create() failed */
            while (1);
        }
    
        retc = sem_init(&semErrorCallback, 0, 0);
        if (retc == -1) {
            /* sem_init() failed */
            while (1);
        }
    
        /* Wait forever for an error */
        sem_wait(&semErrorCallback);
    
        /* Cancel the echo thread (blocks until the thread is closed) */
        pthread_cancel(&thread0);
    
        /* Close the driver */
        I2S_stopClocks(i2sHandle);
        I2S_close(i2sHandle);
    
        /* End this task */
        return NULL;
    }
    

  • Hi Vinay,

    I am not sure to understand your request. I am under the impression you are saying that everything works as expected, is it correct?

    How can we help you?

    Best regards,

  • No Clement, after your modification suggestions i wanted to invoke onboard microphone, which is not working (buffer is not getting any data).

    So if you can review the code above, and point me if any mistakes are there then that would help.

  • Hi,

    We will review the code as soon as possible.

    Please confirm you manage to enable the onboard microphone for echo operation.

    Best regards,

  • Yes clement, in I2S echo example with following changes :  

    #define INPUT_OPTION                    AudioCodec_MIC_ONBOARD

    and while configuring  changing code as below

    /* Configure Codec */
    status = AudioCodec_config(AudioCodec_TI_3254, AudioCodec_16_BIT,
    SAMPLE_RATE, AudioCodec_STEREO, AudioCodec_SPEAKER_HP,
    INPUT_OPTION);

    worked smoothly, where onboardmic could echo back to SPEAKER_LINE_OUT.

  • As mentioned earlier we are looking for onboard microphone samples in RAM worth of 1.5sec data. This is where the code changes suggested were made and still no luck on getting onbaord mic data.

    Would be great if you could review my code as posted above.

  • Hi,

    Please use a logic analyzer to verify on which channel (i.e. on which WCLK polarity) the data is inputted to the CC1352P7 device.

    With the configuration I have, the following code needs to be modified (otherwise the device sample on the "wrong" channel):

    //i2sParams.SD1Channels          = I2S_CHANNELS_MONO;
    i2sParams.SD1Channels          = I2S_CHANNELS_MONO_INV;

    Best regards,

  • Thanks Clement