Tool/software:
I would like to do a simple program:
Wake up from a GPIO, emit a packet, go to sleep, and so on.
Based on the example rfPacketTx and rfPacketRx it works.
void SendPacket(void)
{
RCL_init();
rclHandle = RCL_open(&rclClient, &LRF_config);
rclPacketTxCmdGenericTx.rfFrequency = FREQUENCY;
/* Start command as soon as possible */
rclPacketTxCmdGenericTx.common.scheduling = RCL_Schedule_Now;
rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
rclPacketTxCmdGenericTx.config.fsOff = FS_OFF; // Turn off FS
/* Callback triggers on last command done */
rclPacketTxCmdGenericTx.common.runtime.callback = defaultCallback;
rclPacketTxCmdGenericTx.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value;
/* Set RCL TX buffer packet to be packet buffer */
txPacket = (RCL_Buffer_TxBuffer *)&packet;
// Create packet with random payload
uint8_t *txData;
txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH);
// Zero out data in header before the length field
for (int s = 0; s < LEN_INDEX; s++)
{
txData[s] = 0U;
}
// Set the packet length
txData[LEN_INDEX] = MAX_LENGTH;
// Generate a random payload
for (int i = HDR_LEN; i < MAX_LENGTH; i++)
{
txData[i] = rand();
}
// Set packet to transmit
RCL_TxBuffer_put(&rclPacketTxCmdGenericTx.txBuffers, txPacket);
rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
// Submit command
RCL_Command_submit(rclHandle, &rclPacketTxCmdGenericTx);
//Pend on command completion
RCL_Command_pend(&rclPacketTxCmdGenericTx);
while(!gCmdDone)
{};
gCmdDone = 0;
RCL_close(rclHandle);
}
Now I would like to separate the program into two parts:
The following function is run once at the beginning of the program:
void Init(void)
{
RCL_init();
rclHandle = RCL_open(&rclClient, &LRF_config);
rclPacketTxCmdGenericTx.rfFrequency = FREQUENCY;
// Start command as soon as possible
rclPacketTxCmdGenericTx.common.scheduling = RCL_Schedule_Now;
rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
rclPacketTxCmdGenericTx.config.fsOff = FS_OFF; // Turn off FS
// Callback triggers on last command done
rclPacketTxCmdGenericTx.common.runtime.callback = defaultCallback;
rclPacketTxCmdGenericTx.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value;
// Set RCL TX buffer packet to be packet buffer
txPacket = (RCL_Buffer_TxBuffer *)&packet;
}
The following function is run at every wake-up by the GPIO:
void SendPacket(void)
{
// Create packet with random payload
uint8_t *txData;
txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH);
// Zero out data in header before the length field
for (int s = 0; s < LEN_INDEX; s++)
{
txData[s] = 0U;
}
// Set the packet length
txData[LEN_INDEX] = MAX_LENGTH;
// Generate a random payload
for (int i = HDR_LEN; i < MAX_LENGTH; i++)
{
txData[i] = rand();
}
// Set packet to transmit
RCL_TxBuffer_put(&rclPacketTxCmdGenericTx.txBuffers, txPacket);
rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle;
// Submit command
RCL_Command_submit(rclHandle, &rclPacketTxCmdGenericTx);
//Pend on command completion
RCL_Command_pend(&rclPacketTxCmdGenericTx);
while(!gCmdDone)
{};
gCmdDone = 0;
}
The program seems to run, but it doesn't work. The packet is never received.
Is it mandatory to make an initialization of the RCL each time the processor is woke-up from sleep to emit a new packet?
Regards,
Laurent
Hi Laurent,
Is it mandatory to make an initialization of the RCL each time the processor is woke-up from sleep to emit a new packet?
No, you don't need to do RCL_init/open for every packet.
From my initial look, your code should work, since your SendPacket is doing everything as shown in the while(1) loop of the rfPacketTx.c
Is this program doing ONLY TX (similar to rfPacketTx)? Or does it also do RX?
Maybe you can try the rfEchoTx and rfEchoRx examples?
(Since these only call the RCL_init/open one time also).
Thanks,
Toby
Hi Toby,
This program is only doing Tx.
If I use rfPacketTx and rfPacketRx with no modification, it works.
I made a modification to the rfPacketTx (see below) that goes to sleep and wakes up when you push the btn2 of the LP-EM-CC2340R5.
You can see the LED blinking when you push the button, but nothing is received.
I'm probably missing something with the configuration.
Best Regards,
Laurent
/* * Copyright (c) 2013-2022, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. */ /***** Includes *****/ /* Standard C Libraries */ #include <stdlib.h> #include <stdio.h> #include <unistd.h> #include <limits.h> /* TI Drivers */ #include <ti/drivers/GPIO.h> #include <ti/drivers/rcl/RCL.h> #include <ti/drivers/rcl/RCL_Scheduler.h> #include <ti/drivers/rcl/commands/generic.h> /* SysConfig Generated */ #include "ti_drivers_config.h" #include "ti_radio_config.h" /***** Defines *****/ /* Packet TX Configuration */ #define MAX_LENGTH (30U) // Max packet length #define NUM_DATA_ENTRIES (2U) // Number of data entries #define NUM_PAD_BYTES (3U) // Number of pad bytes #define PACKET_INTERVAL 500000 // Set packet interval to 500000us or 500ms /* The index of the length in the TX packet and the length of the header */ #define LEN_INDEX (RCL_REGISTER_FIELD_PBE_GENERIC_RAM_LENCFG_LENPOS/CHAR_BIT) #define HDR_LEN (LEN_INDEX + (RCL_REGISTER_FIELD_PBE_GENERIC_RAM_LENCFG_NUMLENBITS/CHAR_BIT)) /* Indicates if FS is off */ #define FS_OFF (1U) // 0: On, 1: Off #define FREQUENCY (2440000000U) /***** Variable declarations *****/ /* RCL Commands */ extern RCL_CmdGenericTx rclPacketTxCmdGenericTx; /* RCL Client used to open RCL */ static RCL_Client rclClient; /* TX packet buffer */ uint32_t packet[NUM_DATA_ENTRIES][3 + ((MAX_LENGTH + 10)/ 4)]; /* Counters for RCL event callback */ volatile uint32_t gCmdDone = 0; // Command done volatile uint32_t Count = 0; /***** Callback Functions *****/ void defaultCallback(RCL_Command *cmd, LRF_Events lrfEvents, RCL_Events rclEvents) { if (rclEvents.lastCmdDone) { gCmdDone += 1; GPIO_toggle(CONFIG_GPIO_GLED); } } void BTN_2WakeupCallback(uint_least8_t index) { Count++; } /***** Function definitions *****/ void *mainThread(void *arg0) { /* Initialize and open RCL */ RCL_init(); RCL_Handle rclHandle = RCL_open(&rclClient, &LRF_config); /* Set RF frequency */ rclPacketTxCmdGenericTx.rfFrequency = FREQUENCY; /* Start command as soon as possible */ rclPacketTxCmdGenericTx.common.scheduling = RCL_Schedule_Now; rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle; rclPacketTxCmdGenericTx.config.fsOff = FS_OFF; // Turn off FS /* Callback triggers on last command done */ rclPacketTxCmdGenericTx.common.runtime.callback = defaultCallback; rclPacketTxCmdGenericTx.common.runtime.rclCallbackMask.value = RCL_EventLastCmdDone.value; /* Set RCL TX buffer packet to be packet buffer */ RCL_Buffer_TxBuffer *txPacket = (RCL_Buffer_TxBuffer *)&packet; GPIO_setConfig(CONFIG_GPIO_GLED, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW); GPIO_write(CONFIG_GPIO_GLED, CONFIG_GPIO_LED_OFF); // add the btn2 of the lp-emcc2340r5 to wake-up from sleep GPIO_setConfig(BTN_2, GPIO_CFG_IN_PU | GPIO_CFG_IN_INT_FALLING); GPIO_setCallback(BTN_2, BTN_2WakeupCallback); GPIO_enableInt(BTN_2); while(1) { Power_sleep(PowerLPF3_ENTERING_STANDBY); // PowerCC2340_IDLE, PowerCC2340_STANDBY, /* Create packet with random payload */ uint8_t *txData; txData = RCL_TxBuffer_init(txPacket, NUM_PAD_BYTES, HDR_LEN, MAX_LENGTH); /* Zero out data in header before the length field */ for (int s = 0; s < LEN_INDEX; s++) { txData[s] = 0U; } /* Set the packet length */ txData[LEN_INDEX] = MAX_LENGTH; /* Generate a random payload */ for (int i = HDR_LEN; i < MAX_LENGTH; i++) { txData[i] = rand(); } /* Set packet to transmit */ RCL_TxBuffer_put(&rclPacketTxCmdGenericTx.txBuffers, txPacket); rclPacketTxCmdGenericTx.common.status = RCL_CommandStatus_Idle; /* Submit command */ RCL_Command_submit(rclHandle, &rclPacketTxCmdGenericTx); /* Pend on command completion */ RCL_Command_pend(&rclPacketTxCmdGenericTx); /// usleep(PACKET_INTERVAL); } }
Hi Laurent,
Thanks for sharing more details/code, and apologies for my delay.
The main issue I see in your code is that it explicitly calls "Power_sleep". This should not be done, as it could interfere with the automatic power management integrated with the RTOS (FreeRTOS). (More details described here: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1439063/lp-em-cc2340r5-after-putting-device-in-standby-mode-code-continues-running/5542530#5542530)
I went ahead and combined some examples/drivers together (rfPacketTx + gpioInterrupt + semaphore), and it seems to meet your initial requirements "Wake up from a GPIO, emit a packet, go to sleep".
The zip is attached. They should run ok on a pair of LP-EM-CC2340R5.
/cfs-file/__key/communityserver-discussions-components-files/667/example_5F00_pair.zip
Thanks,
Toby
Hello Toby,
Your code work as expected. Thanks.
I still have a problem : I would like to use a RTC timer to wake up the processor.
I use the code :
#define RTC_PERIOD_MS 3000 #define RTC_FREQ 31250 // 31.25 kHz HwiP_Struct rtcHwi; void rtcInterruptHandler(uintptr_t arg) { if (HWREG(RTC_BASE + RTC_O_RIS) & RTC_RIS_EV0) { HWREG(RTC_BASE + RTC_O_ICLR) |= RTC_RIS_EV0; GPIO_toggle(CONFIG_GPIO_LED_GREEN); HWREG(RTC_BASE + RTC_O_CTL) |= RTC_CTL_RST; } } void rtcInit(void) { uint32_t rtc_interval = RTC_PERIOD_MS * (RTC_FREQ / 1000); HWREG(RTC_BASE + RTC_O_CH0CC8U) = rtc_interval; HWREG(RTC_BASE + RTC_O_IMASK) |= RTC_RIS_EV0; HwiP_construct(&rtcHwi, INT_CPUIRQ0, rtcInterruptHandler, NULL); HwiP_enableInterrupt(INT_CPUIRQ0); HWREG(RTC_BASE + RTC_O_CTL) |= RTC_CTL_RST; HWREG(RTC_BASE + RTC_O_CTL) &= ~RTC_CTL_RST; }
This code was found in thread : https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1442276/lp-em-cc2340r5-rts-timer-waking-up-from-standby-by-rtc-timer
But no interrupt occurs.
My low frequency clock configuration is :
If I read register HWREG(RTC_BASE + RTC_O_TIME8U) or HWREG(RTC_BASE + RTC_O_TIME524M) I can see the value changing. It means that RTC clock is working.
Is there anything missing from the timer configuration?
Best regards,
Laurent
Hi Laurent,
Thanks for the update! Glad to hear it is working.
Regarding wake on RTC, you just need to call sleep(your_sleep_time_sec) or usleep(your_sleep_time_usec).
The RTOS layers will handle wakeup automatically, and this is based on RTC.
Thanks,
Toby
Toby,
I'm going to try your solution with usleep, but there are some links with input interrupt.
With the RTC if I set the bit HWREG(RTC_BASE + RTC_O_ISET) |= 1 and I read HWREG(RTC_BASE + RTC_O_RIS) the bit is set to 1.
It means that the interrupt occurs, but the callback function is not triggered.
Regards,
Laurent
Do you plan to use an RTOS in this application?
If yes, you can use a posix-compatible FreeRTOS timer routine implementation here: C:\ti\simplelink_lowpower_f3_sdk_8_20_00_119\source\ti\posix\freertos\timer.c
This can call a user-specified callback upon timeout.
RTOS does use RTC timer. For example, scheduling its next wakeup which has dependency on timer routines.
Hello Toby,
I succeeded in solving my problem with a simple sleep, as you advised me.
Thank you for your help.
Regards,
Laurent