This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Not sure if you mean the noise floor or the noise figure (NF is typically used for noise figure).
CC1120 Noise Figure (NF) is 6.5 - 7 dB
Noise floor = -174 dBm + 10*log(RX BW) + NF, where RX BW is the receiver filter bandwidth you program into the chip
Sverre,
It was jsut typo, thank you for this information.
Best Regards,
Enok
Thank you for the response. The reason I wanted to double check was because there are differences in the sensitivity and blocking characteristics of the CC1120 compared with the cc1125 and I was wondering if there might also be a difference in the noise figure?
Kind regards
Elliot